Execute Immunity Test via gRPC Service

Be sure to follow the steps below to execute the Immunity Test via gRPC service.

Make sure you have configured the instrument before performing the following steps. If you have not already configured the instrument, run ImplementConfig Function of GeneralInstrumentsAPI.proto.

Step 1: Run loadImmunityTestFile Funtion.

To load the specified Immunity test file into the AC Source application.

Step 2: Execute runImmunityTest Function.

To run the Immunity test.

See Also

gRPC Service

Using gRPC Service

PWACImmunityAPI.proto